Edmund Optics uses cookies to optimize and enhance the features and content on our website. Click “OK” for the full user experience, you can view additional information on the cookies we use by clicking the “Details” button. We do NOT sell your information from marketing cookies, we use it to improve ONLY YOUR experience with Edmund Optics.
We do not use cookies of this type.
Cookies are small text files that can be used by websites to make a user's experience more efficient.
The law states that we can store cookies on your device if they are strictly necessary for the operation of this site. For all other types of cookies we need your permission.
This site uses different types of cookies. Some cookies are placed by third party services that appear on our pages.
You can at any time change or withdraw your consent from the Cookie Declaration on our website.
Learn more about who we are, how you can contact us and how we process personal data in our Privacy Policy.
Please state your consent ID and date when you contact us regarding your consent.
Most web browsers allow you to view your cookies in the browser preferences, typically within the "Privacy" or "Security" tab. Some browsers allow you to delete specific cookies or even prevent cookies from being created. While disallowing cookies in your browser may provide a higher level of privacy, it is not recommended since many websites require cookies to function properly. Alternatively, you can visit www.aboutcookies.org which provides directions on how to block or delete cookies on all major browsers.
|
Single-material aspheric achromats correct for chromatic aberrations using a unique geometry. |
|
Achromatic lenses are typically composed of two or more materials to correct for color. |
|
These unique lenses are achromatic over a wider wavelength range than traditional doublets. |
|
These cement-free achromats open new applications previously limited by the adhesive. |
Achromatic lenses are some of the most commonly used optical components. Historically, they have consisted of two lens elements cemented together to correct for chromatic aberration and bring at least two wavelengths of light to a common point of focus. Single-material aspheric achromats are a novel type of lens that break that assumed rule by using a unique geometry, rather than multiple materials, for achromatic performance. They feature a broader bandwidth than traditional achromats, no coefficient of thermal expansion (CTE) difference between multiple materials, and compatibility with high-power lasers because no cement is required to bond multiple materials.
Achromatic lenses are typically composed of two lens elements cemented together: a positive crown glass element with a low refractive index and a negative flint glass element with a high refractive index. Single-material aspheric achromats circumvent the need to use multiple materials through an innovative and complex aspheric geometry (Figure 1).
Figure 1: Layout of a single-material aspheric achromat from MATLAB. Only half of the lens aperture is illustrated.
Designing and optimizing these lenses required custom optical design code to be developed because available optical design programs, such as Zemax OpticStudio® and Synopsis’ Code V, lacked the ability to define these complex aspheric surfaces. The custom MATLAB code features a higher degree of design freedom by avoiding constraints of the commonly-accepted mathematical representations of aspheric surfaces. More details on custom code development can be found in our published conference proceedings from SPIE LASE 2020.1
Single-material aspheric achromats offer a number of benefits over conventional, multiple-material achromats. Minimizing chromatic focal shift is of particular concern for achromatic lenses, as it is typically desired to have multiple wavelengths focus at a single spot on the optical axis with minimal chromatic spread of other intra-band wavelengths. Figure 2 compares the nominal chromatic focal shift of a single material achromat and an equivalent traditional doublet, revealing that the single material achromat significantly outperforms the conventional doublet on axis.
Figure 2: The 10 µm nominal chromatic focal shift of a 100mm focal length, 0.097 NA single material achromat is a 20X improvement over the 200µm nominal chromatic focal shift of #32-327, a 100mm focal length, 0.013 NA achromatic doublet.
Single material achromats are compatible with higher-power lasers over conventional multiple material achromats, primarily because no optical cement is required to bond different materials. The laser damage threshold of the cement is typically the limiting factor for the laser damage threshold of conventional achromatic doublets.2
The lack of cement also makes single material achromats more thermally stable, as there are no CTE differences between multiple materials. CTE differences between the crown and flint glasses in a conventional achromatic doublet may lead to thermally-induced stress and defocus.
The unique geometry of single-material achromats makes them more difficult to manufacture than many other optical components. Edmund Optics® has been diamond turning single-material achromats out of Zeonex E48R, a commonly used optical plastic; they can also be diamond-turned from other materials, including germanium and silicon.
These lenses must be manufactured through diamond turning, rather than conventional grinding and polishing, to form the required geometry. Some iteration is required to fine-tune the alignment between the front and back surfaces. This is accomplished through a feedback loop of profilometry data and kinematic location of diamond-turned datum including flat annular zones and the outer diameter.1
To evaluate how closely the performance of the manufactured single-material achromats matched their nominal performance, the chromatic focal shift of 18 sample lenses was determined by measuring the position of best focus at different wavelengths from 450-650nm using an Optikos MTF test bench and a series of 10nm bandwidth optical filters, as shown in Figure 2. Full details of the testing can be found in the SPIE LASE 2020 conference proceedings.1
The chromatic focal shift values of the 18 single-material aspheric achromat samples ranged from 49 to 75µm. For reference, the equivalent achromatic doublet from Figure 2 was measured using an identical method and had a chromatic focal shift of around 210µm. While the single-material achromats had some performance degradation due to manufacturing tolerances when compared to their nominal performance, they significantly outperformed the conventional achromatic doublet by a factor of three (Figure 3).
Figure 3: Comparison of the measured chromatic focal shift of 18 different single-material achromatic lenses with that of a traditional achromatic doublet shows that the single-material achromats have significantly less chromatic focal shift
They must be made out of a material that can be diamond-turned, as conventional grinding and polishing cannot achieve the required complex geometry. Edmund Optics® has made single-material aspheric achromats out of Zeonex E48R, but germanium, silicon, and other materials that can be diamond-turned could also be used.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2024, Edmund Optics Singapore Pte. Ltd, 18 Woodlands Loop #04-00, Singapore 738100
California Consumer Privacy Acts (CCPA): Do Not Sell or Share My Personal Information
California Transparency in Supply Chains Act